Technical FAQs

Ask a Question

On a 9001B standard control station, the universal selector switch unit lists contact symbol 17 or 19. How can it have both?

The selector switch is convertible from between 2 position and 3 position. When used as 2 position, it uses contact symbol 19. As a 3 position switch, it uses contact symbol 17.


CTA-ID : 2026548
Was this helpful?
What can we do to improve the information ?