Technical FAQs

Ask a Question

How can the AOC output terminal be set up as a logic output in an Altivar 31 drive?

In the IO menu, set AOIt to 0A and then set dO to the desired logic output function such as rUn, Drive Running.  The logic output state is 1 (24V) when the selected assignment is active, except for FLt, which is powered up if the drive is not faulted.
See the Altivar 31 Programming manual for more information regarding the settings.
See the Altivar 31 Installation manual for more information regarding the ratings of the output.

Reviewed 8/2011


CTA-ID : 2025883
Was this helpful?
What can we do to improve the information ?