Technical FAQs

Ask a Question

Can a 480V Breaker be used on a 380V System?

Yes. Breakers can be applied at voltages less than their rating, but not more than their ratings.
In the case of GFI, EPD, and AFI breakers, available voltage must be greater than 100 Vac.

CTA-ID : 2026530
Was this helpful?
What can we do to improve the information ?