Technical FAQs

Ask a Question

Is it possible to order a QO342MQ150 load center with a 70A main breaker instead of the 150A main breaker?

Yes. Order catalog number QO342MQ15070. The device is a special, so contact 1-888-778-2733 for ordering information.

CTA-ID : 2026528
Was this helpful?
What can we do to improve the information ?