Technical FAQs

Ask a Question

How do you wire the SDSA1175?

Connect the white on the neutral bar in the panel.
Connect the black wires to the phase lugs or phase wires by an NEC approved method (we recommend connecting to a 30 A, 2p branch breaker).

Refer to attached instruction bulletin.


CTA-ID : 2025949
Was this helpful?
What can we do to improve the information ?