Technical FAQs

Ask a Question

What is the torque requirement for the lugs on a SN1200NA?

Issue:
Torque spec

Product Line:
Enclosed Breakers

Environment:
NAL,NCL,NXL

Cause:
Installation

Resolution:

The neutral lugs (#3/0 - 600 kcmil) should be torqued to 330 inch pounds. The service ground lug (#4 - 300 kcmil) should be torqued to 250 inch pounds.


CTA-ID : 2026110
Was this helpful?
What can we do to improve the information ?