Technical FAQs

Ask a Question

What would cause an incoming section to be added for a single main HVL N3R switch?

In some cases if a full height rear cable barrier is required and the cable sizes require both line-side and load-side rear connector assemblies, the incoming section is required. Standard line and load connectors interfere with each other.

This problem can be solved with special make assemblies.
Was this helpful?
What can we do to improve the information ?