Technical FAQs

Ask a Question

Is the DB chopper part of the Altivar ATV66 drive or does it need to added it externally?

All ATV66 models have a built-in DB chopper except for the ATV66C10-C19N4U drives.
These exceptions do not have the DB chopper unless they are ordered with ``.....BU`` at the end of the part number.


CTA-ID : 7138
Was this helpful?
What can we do to improve the information ?