Technical FAQs

Ask a Question

Does Square D have UL listed power fuses for metal enclosed switchgear?

Some of the fuses are UL listed and some are not. Ferraz Shawmut fuses are UL listed. Cooper Bussman DIN/E Type fuses are not UL Listed. It is NOT required to use a UL listed power fuse installed in a UL labeled HVL or HVL/cc.


CTA-ID : 2025937
Was this helpful?
What can we do to improve the information ?