Technical FAQs

Ask a Question

ATV58 What is the range for the analog output for motor power based on?

On this parameter OPr, the maximum value is 200 % of the nominal power of the drive based on the Constant Torque Ratings for most ATV58 drives. For The ATV58HC10N4 and larger, it is 200% of the nominal power of the drive based on the Variable Torque Ratings.


CTA-ID : 2026313
Was this helpful?
What can we do to improve the information ?