Technical FAQs

Ask a Question

What is the permissible wire range of the power terminals on the Class 8903 Type SQ 100 amp lighting contactor?

Those lugs will accept a single conductor, #14 to 2/0 copper or aluminum wire.

CTA-ID : 2011734
Was this helpful?
What can we do to improve the information ?