Technical FAQs

Ask a Question

What is the difference between a PAK11C and PAK11C1?

In a PAK11C1, breakers and receptacles are located together behind the outer door, which is padlockable. With a PAK11C, breakers and receptacles are separated from each other: the breakers are behind the outer door, and the receptacles are located in the bottom end wall in such a way that they are available with the outer door padlocked. There is also a minimum order quantity of fifty for the PAK11C

CTA-ID : 2025927
Was this helpful?
What can we do to improve the information ?