Technical FAQs

Ask a Question

Are the lever arms on a XCKML121 and XCKML521 replacable.

The standard arm is ZCK Y31. ZCK Y33 or ZCK Y34 may be substituted. Other arms may fit the shaft, but not clear the contact body housing.

The head and body are never sold separately as individual components.

CTA-ID : 2026293
Was this helpful?
What can we do to improve the information ?