Technical FAQs

Ask a Question

Is the standard single pole QO type breaker rated at 120 V to ground or 240 V? How about the two pole breakers?

The single pole breakers are rated at 120 V to ground. The two pole breakers are rated at 120 V to ground, but 240 V phase to phase.


CTA-ID : 2026104
Was this helpful?
What can we do to improve the information ?