Technical FAQs

Ask a Question

On the TVSS units what is the difference between the FC and FI?

The difference is the circuit breaker. In the FC unit uses the FC breaker rated t 65KA @480V and FI unit uses a FI breaker rated 200KA @480V.

CTA-ID : 2026492
Was this helpful?
What can we do to improve the information ?