Technical FAQs

Ask a Question

What is the AIR rating for JD breakers?

25K @ 240 Vac, 18K @ 480 Vac, 14K @ 600 Vac and 20K @250 Vdc


CTA-ID : 2026616
Was this helpful?
What can we do to improve the information ?