Technical FAQs

Ask a Question

Can the 100% rated breakers, LEL for example, use 90 degree rated wire loaded per the 90 degree rating tables?

No, the 100% rated breakers do require the use of 90 degree C rating wire but it must be sized to the ratings of 75 degree C wire.

CTA-ID : 2026604
Was this helpful?
What can we do to improve the information ?