Technical FAQs

Ask a Question

What is the part number for a 2 M cord set for the XS2M18MA230K sensor?

Use XSZCK101Y for 90 degree and XSZCK111Y for straight . These cordsets are also recommended for any sensor with a part number ending in ``K``or ``U20``.

CTA-ID : 2026490
Was this helpful?
What can we do to improve the information ?