Technical FAQs

Ask a Question

Are lever bypass meter sockets used with catalog EZML branch devices fully rated for a load break at 225 amps? In other words, can the bypass be opened at full load when the meter has been removed?

No. The bypass is not meant to be opened under load.

CTA-ID : 2026489
Was this helpful?
What can we do to improve the information ?