Technical FAQs

Ask a Question

What is the cross for the ITE K1600 breaker?

The ITE K1600 is the breaker we used to sell as the PB, and is replaced by the Masterpact NW, N rated breaker. It had an AIR of 50 kA @ 480 Vac.
The MP to NW retrofit kit (NW Pricing Guide page 17) can be used with custom field adaptation to fit the K1600 cell.

CTA-ID : 2026488
Was this helpful?
What can we do to improve the information ?