Technical FAQs

Ask a Question

What is the wire capacity of the lugs on a QMB325WT3?

The lugs on this switch will accomodate:
(2) 250 kcmil Al/Cu
(1) 600 kcmil Al/Cu



CTA-ID : 2026483
Was this helpful?
What can we do to improve the information ?