Technical FAQs

Ask a Question

Does the Square D, QO612L100... and QO816L100... (Series G) load centers have the interiors mounted horizontally so the branch breakers go from left-to-right?

Issue:
Product Design Features

Product Line:
QO Load centers

Environment:
Branch breaker orientation

Cause:
Installation

Resolution:

Yes, the interior design of all the QO612L100... and QO816L100... (series G) load centers has a horizontally mounted interior, so the branch circuit breakers will mount on the interior from left-to-right and the circuit breakers operate with the 'ON' in the up position and the 'OFF' in the down position.


CTA-ID : 2026258
Was this helpful?
What can we do to improve the information ?