Technical FAQs

Ask a Question

Will 600V rated plug-in units (such as PQ3603G or PQ3606G) work on a 240V busway run?

Yes. All of the conductors are sized for a 600V maximum circuit. However, you must still use 600V rated fuses, since the fuseclips cannot be changed to accept 240V fuses.


CTA-ID : 2026081
Was this helpful?
What can we do to improve the information ?