Technical FAQs

Ask a Question

What is the wire temperature rating for a HOM circuit breaker?

10 to 30 amp circuit breakers are suitable for use with 60C or 75C conductors. 40 to 200 amp circuit breakers are suitable for use with 75C conductors.


CTA-ID : 2026599
Was this helpful?
What can we do to improve the information ?