Technical FAQs

Ask a Question

What is the wire range for the main lugs on 400 amp NQOD442L400CU?

2- 1/0 to 300 kcmil AL/CU or 1- 1/0 to 750 kcmil AL/Cu


CTA-ID : 2026254
Was this helpful?
What can we do to improve the information ?