Technical FAQs

Ask a Question

What are the dimensions of the enclosure used for UL testing the Powerpact H and J breakers?

Powerpact H (150A) - 18 inches high x 8-1/2 inches wide x 4 inches deep
Powerpact J (250A) - 28 inches high x 12-1/8 inches wide x 5-1/4 inches deep

CTA-ID : 2026520
Was this helpful?
What can we do to improve the information ?