Technical FAQs

Ask a Question

What type of hubs or conduits may be used to feed ANY of the MP METER-PAK meter devices?

Issue:
Product Features

Product Line:
MP Meter Pak metering

Environment:
Enclosure hub openings

Cause:
Application

Resolution:
The MP Dimensions and knockouts for each catalog number are shown in the current digest as the below boxes and also can be seen on each separate catalog number CAD drawing;
For Box 1R, the Top Endwall will accept one Series A Hub and is supplied with a ACP closing plate. The Bottom Endwall will accept one Series A or B300 Hub provision with knockout provisions for
1-1/4", 2.0" and 2-1/2" conduits.

For Box 2R, the Top Endwall will accept one Series A-L Hub and is supplied with a ACPL closing plate. The Bottom Endwall will accept two Series A-L hub provisions with knockout provisions for
1-1/2", 2.0", 2-1/2", 3.0", 3-1/2" and 4.0" conduits. 

For Boxes 3R, 4R, 5R, 6R, 7R, 8R and 9R the Top Endwall will accept two Series A-L Hubs and is supplied with a ACPL closing plate on each hub opening. The Bottom Endwall will accept two Series A-L hub provisions with knockout provisions for 1-1/2", 2.0", 2-1/2", 3.0", 3-1/2" and 4.0" conduits. 



 
Was this helpful?
What can we do to improve the information ?