Technical FAQs

Ask a Question

Is the I-Line HCN panelboard 600V rated or 240V rated?

Issue:
Is the I-Line HCN panelboard 600V rated or 240V rated?

Product Line:
Panelboards

Environment:
I-Line

Cause:
Feature

Resolution:
The panelboard is good up to 600V. The panel is rated only as high as the breakers used in the panel.


CTA-ID : 2026516

Was this helpful?
What can we do to improve the information ?