Technical FAQs

Ask a Question

How many connectors are in the SKNQOD225 kit and what material are they made of ?<br /><br />

This kit contains bus connectors for a 3 pole breaker. (Two A-C connectors and one B connector) . They are tin plated copper connectors for use on interiors with either aluminum or copper bus .


CTA-ID : 2026514
Was this helpful?
What can we do to improve the information ?