Technical FAQs

Ask a Question

On a lever bypass meter socket, why is it not possible to install the meter socket cover with the lever bypass engaged?

A lever bypass is intended to temporarily bypass the meter when utility company personnel are installing or servicing the meter. The meter must be installed and the lever bypass disenganged before the meter socket cover can be secured.


CTA-ID : 2035442
Was this helpful?
What can we do to improve the information ?