Technical FAQs

Ask a Question

What were the design changes to the 200A through 600A Double Throw Switches back in March of 2006?

Issue:
Product Design Changes

Product Line:
Double Throw Safety Switches

Resolution:
New 200 - 600A Double Throw Switches Questions & Answers

Q. What changed?
A. All non-load break switches were replaced with load break designs. See the cross reference in additional FAQ`s. Additionally, all switches are now UL listed and have the ability to field install neutral and electrical interlock kits.

Q. Why did this change happen?
A. Customer preference for load break capability has been added to the UL requirements.

Q. When did this take place?
A. Production of the old non-load break catalog devices stopped on approximately February 24, 2006. After that date only load break devices are being manufactured.

Q. When did inventory become available?
A. Warehouse inventory was changed over to the load break design. All inventories of the non-load break switches were sold on a first come basis until inventory was depleted. Production of the new load break switches began approximately on February 27.

Q. Did the dimensions of the switches change?
A. Yes. Dimensional information was available in March of 2006. SEE CURRENT 2D CAD DRAWINGS FOR CURRENT CATALOG NUMBERS



CTA-ID : 2026594
Was this helpful?
What can we do to improve the information ?