Technical FAQs

Ask a Question

On a QO type GFCI breaker does Square D offer an indicator light option to indicate that the breaker has tripped?

No. Only a mechanical device to indicate circuit breaking tripping on the QO breakers, the Visi Trip indicator, is provided. There are no electrical indicators offered.


CTA-ID : 2026447
Was this helpful?
What can we do to improve the information ?