Technical FAQs

Ask a Question

Can a HU364DS be padlocked in the ON position

As the switch ships from the factory, it can only be locked in the OFF position. In order to modify the switch to allow it to be locked in the ON position, a hole will have to be drilled in the lockplate. This hole should be drilled in the location of the small dimple on the lockplate.


CTA-ID : 2026443
Was this helpful?
What can we do to improve the information ?