Technical FAQs

Ask a Question

Can a QBMIK interlock can be used on two QBA Breaker in an I-line Panelboard?

Issue:
Can a QBMIK interlock can be used on two QBA Breaker in an I-line Panelboard?

Product Line:
I line panelboards and switchboards with I line distribution.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No it won`t mount over the I-Line Breaker Shrouding


CTA-ID : 2026225

Was this helpful?
What can we do to improve the information ?