Technical FAQs

Ask a Question

Can I get a communication module for an NW breaker with a P type trip unit?

The catalog number of the breaker communications module (S48384) comes installed in a breaker with a P type trip unit. The optional cradle communications module is S48377.


CTA-ID : 2026439
Was this helpful?
What can we do to improve the information ?