Technical FAQs

Ask a Question

What are the two heads included with the 9007CB205 multiple unit limit switch?<br /><br />

The 9007CB205 includes two modified 9007C bodies with B heads . An individual replacement head and contact assembly is a 9007CB105 , and two such parts inside a 9007CB20 body make up the whole assembly . Lever arms need to be furnished separately .


CTA-ID : 2025420
Was this helpful?
What can we do to improve the information ?