Technical FAQs

Ask a Question

Is there grounding means supplied with the Class 8538 Type S____ NEMA size 3 through NEMA size 6 combination starters?

Yes, ground connection(s) are provided as standard.


CTA-ID : 2025404
Was this helpful?
What can we do to improve the information ?