Technical FAQs

Ask a Question

What is an XU2P18PL9AB? [Added obsolescence date.]

An XU2P18PLAB and /or XU2P18PL9ABW are special thru beam emitter receiver sensors for Chrysler and are wired for light operate mode only. They both have 4 pin micro connectors. The XU2P18PLAB is a front sensing device. The XU2P18PLABW is a 90 degree side sensing device. These sensors are obsolete at the end of 2006 to comply with the RoHS standard.




CTA-ID : 2025850
Was this helpful?
What can we do to improve the information ?