Technical FAQs

Ask a Question

What are the dimensions and weights of the ATS48C41Y, ATS48C48Y, ATS48C59Y and ATS48C66Y?

These are all the same Frame size:
Width = 15.75 in (400 mm)  
Height = 26.38 in (670 mm)
Depth = 11.81 in (300 mm)
Weight = 113.3 pounds (51.4 kg)

Reviewed 10/2011


CTA-ID : 2025845
Was this helpful?
What can we do to improve the information ?