Technical FAQs

Ask a Question

For ALL the EZM Meter Branch Device catalog numbers with a 'CU' suffix, (Example; EZMH114225CU) what does the suffix 'CU' indicate?

Issue:
Product Catalog number

Product Line:
EZM Metering

Environment:
Catalog logic

Cause:
Bussing material requirement

Resolution:
The suffix "CU" in the catalog numbers indicate all the bussing supplied in the EZM branch device is copper.


CTA-ID : 2025841
Was this helpful?
What can we do to improve the information ?