Technical FAQs

Ask a Question

Can an auxiliary contact be added to the handle operator of a KA225AWK?

The auxiliary contact is an accessory that goes into the circuit breaker itself. It does not go onto the KA225AWK enclosure. Order the KA circuit breaker with the auxiliary contacts factory installed. This breaker will fit into the KA225AWK enclosure.


CTA-ID : 2025840
Was this helpful?
What can we do to improve the information ?