Technical FAQs

Ask a Question

What catalog number suffix is required for the provision of both copper lugs and a 1212 auxiliary switch for FAL circuit breakers?

The suffix for copper lugs is 8002.
The suffix for auxiliary switch is 1212
The combination of 8002 + 1212 = 1214


CTA-ID : 2025738
Was this helpful?
What can we do to improve the information ?