Technical FAQs

Ask a Question

What are the contact ratings of the 9999TC** auxiliary contacts?

This information applies to 9999TC10, 9999TC11, 9999TC20 and 9999TC21 auxiliary electrical interlocks.

Inductive Amperage Ratings based on 35% power factor for 50 and/or 60 hertz applications are as follows:

Volts Make Break Continuous
120 40 15 15
240 20 10 15
480 10 6 15
600 8 5 15

Resistive Amperage Ratings based on 75% power factor for 50 and/or 60 hertz applications are as follows:

Volts Make Break Continuous
120 15 15 15
240 15 15 15
480 15 15 15
600 15 15 15


CTA-ID : 2025736
Was this helpful?
What can we do to improve the information ?