Technical FAQs

Ask a Question

Will the SR1CBL02 programming cable from the older Zelio-Logic SRI relay work with the newer SR2?

Issue:
Will the SR1CBL02 programming cable from the older Zelio-Logic  SRI relay  work with the  newer SR2?

Product Line:
Zelio Relays and Timers

Environment:
All Products

Cause:
Product Features

Resolution:
No, cables are not interchangeable


CTA-ID : 2025399
Was this helpful?
What can we do to improve the information ?