Technical FAQs

Ask a Question

Will the LXL breaker accept all of the following accessories on one breaker:<br />12v DC shunt trip - 1039<br />auxiliary switches - 2A/2B?<br />alarm switch - 2100

Yes. The alarm switch is factory installed only.


CTA-ID : 2025722
Was this helpful?
What can we do to improve the information ?