Technical FAQs

Ask a Question

Can a HOM20L125C main lugs load center be converted to main breaker?

Issue:
Product Design Feature

Product Line:
Homeline Load centers

Environment:
Convert Main lug to Main Breaker

Cause:
Application

Resolution:
It will depend on the Series Number of the load center. The series S is a convertible main device, so a QOM1 frame main breaker kit can be field installed to replace the main lugs. The older design Series 1 or 2 were designed as fixed mains and cannot be converted.


CTA-ID : 2025503
Was this helpful?
What can we do to improve the information ?