Technical FAQs

Ask a Question

Is a NEMA 1, LA400S circuit breaker enclosure available without knockouts?

No, but you may consider using a LA400AWK, a NEMA 12 enclosure. The LA400AWK does not contain knockouts. The LA400AWK will accept only LAL, LHL or Q4L frame circuit breakers.


CTA-ID : 2025497
Was this helpful?
What can we do to improve the information ?