Technical FAQs

Ask a Question

What is necessary to put a NQOD430L225 or NQOD430L225CU MLO interior in a MH44 or MH44WP?<br /><br />

The following parts will be required per panel:

(2) 80110-288-04 12`` rail extensions
(1) 80110-291-04 12`` MLO deadfront extension
(2) 80110-289-01 Deadfront mounting brackets
(2) 80025-067-01 Deadfront screws
(4) 21590-17081 Rail extension screws

Revised 3/10/04




CTA-ID : 2025821
Was this helpful?
What can we do to improve the information ?