Technical FAQs

Ask a Question

What is the part number for a Modbus communication module part number for the PG circuit breaker?

Use the following part numbers:
Unit Mount S64205
I-line S64205
Motor Operated S64207
Drawout S64206
With Rotary Handle S64205



CTA-ID : 2025678
Was this helpful?
What can we do to improve the information ?