Technical FAQs

Ask a Question

Does a sealing ring come with a 29007 meter socket closing plate?

No, the 29007 is a closing plate only. If being used on a ring-type meter socket, you will need to use either a standard snap-type aluminum sealing ring, part number 2920910001, or an optional screw-type aluminum sealing ring, part number 29008W.


CTA-ID : 2025479
Was this helpful?
What can we do to improve the information ?